PsyCalc® Version History
7.0.1
2023-06-05MOD - Hid the External Binning database as its not useful.
7.0.0
2023-06-05MOD - Include data binning. Updated icons, images, and links to the website. Binning databases are now downloadable. The system (starting from here) will automatically update
6.2.0
2023-02-27MOD - Munters name and licensing agreements
6.1.38
2022-11-10 *FIX - Licensing system has been removed.
6.1.37
2022-09-28 *FIX - Point Log save to PDF issues.
6.1.36
2022-08-28 *FIX - Tabbing functionality on PsyCalc, Mixing and Process screens.
6.1.35
2022-08-24 *ADD - Functionality for saving input defaults in Mixing and Process screens.
6.1.34
2022-08-21 *FIX - Minor changes to Binning, Stats and Hourly reports.
6.1.33
2022-08-10 *ADD - Location and binning settings to exported hourly data.
6.1.32
2022-08-05 *ADD - Location and binning settings to exported binned data. ADD - Location and stats settings to exported stats data.
6.1.31
2022-07-25 *FIX - issue importing EPW files from non-USA locations.
6.1.30
2022-07-17 *FIX - issue with WB as an input at high relative humidities.
6.1.29
2022-07-05 *FIX - removed incomplete work contained 6.1.28.
6.1.28
2022-06-23 *FIX - Binner - SI, Joint Frequency binning with 1°C temperature bins was crashing. Please use version 6.1.29 or later.
6.1.27
2022-06-11 *ADD - Binner - Added validation of external data from Excel template.
6.1.26
2022-05-30 *FIX - Binner - Fixed issue with use of external data from Excel template.
6.1.25
2022-05-19 *FIX - ALL - PPM value were being calculated on a dry air basis.
6.1.24
2022-05-09 *FIX - Process - Density value had absolute humidity units.
6.1.23
2022-04-28 *FIX - Process - Onscreen leaving point properties were not updated with elevation/pressure changes.
6.1.22
2022-04-22 *
FIX - Process - Leaving point properties were not updated with elevation/pressure changes.
FIX - Air Flows - Actual vs Standard flows was using density instead of STP.
FIX - Mixing - Error in mixing calculation caused small errors in results.
6.1.21
2022-04-16 *FIX - Binner - Window was opening with Stats panel displayed.
6.1.20
2022-04-05 *FIX - Mixing - Fixed issue with mixing high temperature airstreams.
6.1.19
2022-03-22 *FIX - PsyCalc® - Window scaling factor was not being saved.
6.1.18
2022-03-04 *
FIX - PsyCalc® Mixing - Issue when input value(s) are in actual flow rate.
FIX - PsyCalc® - Window scaling for cultures using comma as decimal separator.
FIX - PsyCalc® Binner & ASHRAE Data - Map component does not support all cultures.
6.1.17
2022-02-14 *
ADD - PsyCalc® Binner - Allow users to Save more than one external data location.
ADD - PsyCalc® Binner - Tabbed VLI panel with design percentiles.
FIX - PsyCalc® Binner- Error message on open for new installations.
6.1.16
2022-02-03 *
ADD - PsyCalc® Binner - Add import for CSV files (TYM3 format)
ADD - Design Data and Binner - Add WMO number mouseover for station dropdown list.
ADD - PsyCalc® Binner - New panel with Ventilation Load Index calculated.
ADD - Defaults - Allow user to change window scaling factor.
FIX - PsyCalc® Binner - Corrected humidity ratio conversion was using wind speed value.
6.1.15
2022-01-26 *FIX - Process - corrected issue calculating results when actual flow values are used.
6.1.14
2022-01-10 *MISC - Minor house-keeping & code clean-up, additional logging.
6.1.13
2022-01-02 *FIX - PsyCalc, Mixing and Process - corrected issue limiting minimum pressure input.
6.1.12
2021-12-23 *FIX - Cool/Heat comparison - corrected some units of measure labels.
6.1.11
2021-12-12 *FIX - Find Locations - corrected some units of measure issues.
6.1.10
2021-12-01 *FIX - PsyCalc® Binner window - Download Hourly Data button was not visible.
6.1.9
2021-11-21 *
FIX - Changing input units of measure in mixing screen produced an error in results.
FIX - Changing Airstream A air flow value in mixing screen was not updating Ratio % values.
6.1.8
2021-11-14 *FIX - Changing to SI inputs in mixing screen was blanking out output grid.
6.1.7
2021-11-04 *Add - Edit / Copy Window - Places a bitmap image of the current window on the clipboard.
6.1.6
2021-10-18 *Add - ASHRAE Design Data - Add extreme wet bulb temperatures in Historical section.
6.1.5
2021-10-07 *
FIX - Mix window - blank out output if mix is super saturated.
Add- Help menu - Add link to online version log.
FIX - Mix window - fixed error in reverse mixing functionality.
6.1.4
2021-09-26 *
NEW - PsyCalc® Binner - Output bins by month in addition to annual bins.
NEW - Process window - Enable save to log functionality for point-to-point and defined process types.
6.1.3
2021-09-10 *
NEW - PsyCalc® Binner - Add TMY2 and EPW file types to external data import functionality.
NEW - PsyCalc® Binner - View summary data about all hours above or below any bin. Just right click a bin row and chose from the popup menu
6.1.2
2021-08-20 *Fix - Process window - default units of measure were not being respected in HVAC Components windows.
6.1.1
2021-08-02 *
NEW - For Standard bins - right click on a binning results row to see cummulative stats for values above or below the row mid-point.
Fix - Process window - values in the output grid were not being updated when changing output units.
Fix - PsyCalc Binner - on the Stats panel decimal separators other than a point were causing an error.
6.1.0
2021-07-14 *
Update - ASHRAE Climatic Design Data from the 2013 dataset to the 2017 dataset. PsyCalc® now has the latest set of this data increasing the number of locations from 6,443 to 8,118. This data is provided under license from ASHRAE.
NEW - Functionality to allow users to use external hourly weather data from recognized sources or an Excel template provided with this update.
Change - Changing input property types on Point, Mixing and Process screens by default does not update the corresponding value. This behavior is the same as all previous versions of PsyCalc®. Users can override this bahavior in Defaults / General by checking the Update input value when changing input type checkbox.
Fix - Some minor bug fixes, spelling errors, etc.
NEW - Added a button in Defaults / Binning Data to open a web page where all hourly weather data files can be downloaded after some users reported an issue using the individual download buttons.
6.0.0
2021-06-30 *Initial release of 20th Anniversay Edition